Configure Jitter Measurements

Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4

Use the Jitter Mode Measurements Setup dialog to modify how FlexDCA performs and reports Jitter Mode measurements. For example, you can jitter select jitter measurements to be reported in either seconds or unit intervals. Or, you could change the sampling levels (Thresholds) at which a signal's jitter level or amplitude location is determined.