Amplitude Toolbar
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Jitter mode displays a set of default graphs at the top of the screen. To select which amplitude (interference) graphs to display, click the graph buttons that are found on the Amplitude Toolbar. Click the following selections to learn about each available graph.
Measurement results are not reported until a significant sample size of data is acquired. Click Measure > Configure Jitter Mode Measurements to configure the measurements. For PAM4 signals, many graphs can be based on a specific level.
Many amplitude graphs show results based on amplitude levels. To change the level that is graphed, do one of the following:
- Click the graph's Cycle Eye button.
- Change the Graphs Based on setting in the Amplitude Measurements tab of the Configure Jitter Measurements dialog.