NRZ Measurement Panels

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Amplitude

The Jitter and Amplitude results panels are displayed whenever an NRZ signal has been detected. Specific measurements on the toolbar are disabled if the format of your waveform is not NRZ and the measurement is not compatible with NRZ. By default, the Jitter and Amplitude panels include a standard set of scalar measurement. Additional measurements can be added to a panel by clicking the measurement buttons that are available on the Meas toolbar.

To reset the panels to their default measurements, click the Reset Jitter and Reset Amplitude buttons.

In the upper-right corner of the panel, the LJM and SP annotations may appear to indicate the presence of Large Jitter Mode or a Signal Processed waveform respectively.

If the Amplitude panel is not displayed, click the Measure > Jitter > Amplitude > Amplitude Meas ON.

Jitter Table Measurements
Measurement Name Remote Command Additional Information
Default Measurements
DCD :MEAS:JITT:DCD For NRZ signals only.
DDJ (p-p) :MEAS:JITT:DDJ
DJ (δ-δ) :MEAS:JITT:DJ
Eye Width :MEAS:JITT:EWIDth
ISI-J (p-p) :MEAS:JITT:ISI
PJ (δ-δ) :MEAS:JITT:PJ Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Spectral.
BUJ (δ-δ) Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Auto or Tail Fit.
PJ (rms) :MEAS:JITT:PJRMs Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Spectral.
BUJ (rms) Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Auto or Tail Fit.
RJ (rms) :MEAS:JITT:RJ
TJ :MEAS:JITT:TJ
Additional Measurements on Meas Toolbar
DDPWS :MEAS:JITT:DDPWs For NRZ signals only.
F/2 (p-p) :MEAS:JITT:FOVer2
JN :MEAS:JITT:JN
Meas. Level :MEAS:JITT:LEVel This measurement is only shown in the panel by sending the remote command.
UJ (rms) :MEAS:JITT:UJ
Amplitude Table Measurements
Measurement Name Remote Command Additional Information
Default Measurements
DI (δ-δ) :MEAS:AMPLitude:DI
Eye Height :MEAS:AMPLitude:EHEight
ISI (p-p) :MEAS:AMPLitude:ISI
Level :MEAS:AMPLitude:LEVel
PI (δ-δ) :MEAS:AMPLitude:PI Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to the default Spectral selection.
BUI (δ-δ) Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Auto or Tail Fit.
PI (rms) :MEAS:AMPLitude:PIR Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to the default Spectral selection.
BUI (rms) Available when Separation Method setting in the Advanced tab of the Jitter Mode Measurements Setup dialog is set to Auto or Tail Fit.
Q :MEAS:AMPLitude:Q
RN (rms) :MEAS:AMPLitude:RN
Signal Amplitude :MEAS:AMPLitude:SAMPlitude For electrical signals.
Mod'n Amplitude For optical signals (in Watts).
SER Floor :MEAS:AMPLitude:SERFloor
SER Limit :MEAS:AMPLitude:SERLimit
TI :MEAS:AMPLitude:TI
VEC :MEASure:AMPLitude:VECLosure IEEE 802.3ck compatible Vertical Eye Closure
Additional Measurements on Meas Toolbar
De-Emphasis (PCIe) :MEAS:AMPLitude:DEPCie For NRZ signals only.
Eye Opening :MEAS:AMPLitude:EOPening This measuurement is only shown in the panel by sending the remote command.
Highest :MEAS:AMPLitude:HSYMbol This measuurement is only shown in the panel by sending the remote command.
Lowest :MEAS:AMPLitude:LSYMbol This measuurement is only shown in the panel by sending the remote command.
Preshoot (PCIe) :MEAS:AMPLitude:PPCie For NRZ signals only.
RIN :MEAS:AMPLitude:RINoise
UN (rms) :MEAS:AMPLitude:UN

Data Acquisition Delays

Normally, data acquisition and measurement happens very quickly. As soon as the graphs scroll over the screen, the results are displayed. If, however, you are measuring very long patterns (for example, 216–1 PRBS), you may notice a delay between the time when the graphs scroll down and the final results are displayed in the panels. How can you tell when your measurements are finished? Look for the measurement annotations in the Jitter and Amplitude panels. The text "No Data" next to an entry indicates the edges are being characterized. A question mark (?) next to a measurement result indicates that indicates a measurement in process.

Waveform Compatibility

Jitter Measurements and Supported Waveforms
Measurement Waveform Types
NRZ PAM4 PAM6 PAM8
DCD ●  
DDJ (p-p) ●  
DJ (δ-δ) ●  
Eye Width ●  
ISI-J (p-p) ●  
PJ (δ-δ) / BUJ (δ-δ) ●  
PJ (rms) / BUJ (rms) ●  
RJ (rms) ●
TJ ●
DDPWS ●  
F/2 (p-p) ●
J2 ●
Meas. Level ●
UJ (rms) ●
Amplitude Measurements and Supported Waveforms
Measurement Waveform Types
NRZ PAM4 PAM6 PAM8
DI (δ-δ) Ones ●  
DI (δ-δ) Zeros ●  
Eye Height ●
ISI (p-p) Ones ●
ISI (p-p) Zeros ●
One Level ●
Zero Level ●
PI (δ-δ) / BUI (δ-δ) Ones ●
PI (δ-δ) / BUI (δ-δ) Zeros ●
PI (rms) / BUI (rms) Ones ●
PI (rms) / BUI (rms) Zeros ●
Q ●
RN (rms) Ones ●
RN (rms) Zeros ●
Mod'n Amplitude (Signal Amp) ●
SER Floor ●
SER Limit ●
TI Ones ●
TI Zeros ●
VEC ●
De-Emphasis (PCIe) ●  
Preshoot (PCIe) ●
RIN ●
UN (rms) Ones ●
UN (rms) Zeros ●