Limit Testing

Instrument
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR

Limit testing allows you to stop data acquisition based on one of the following four types of events. When the specified limit conditions are met, the active tasks stop and, if defined, a reporting action is taken for each limit test.

To select and configure limit testing, click Measure > Limit Tests. The following table shows the availability of each type of limit test according to instrument modes.

Availability of Limit Tests
Type of Limit Test Instrument Mode
Oscilloscope Eye/Mask TDR/TDT Jitter
Acquisition Limits ♦ ♦ ♦ ♦
Measurement Limits ♦ ♦ ♦ ♦
Limit-Line-Test Limits ♦ ♦
Mask-Test Limits ♦

You can run one or more limit tests at a time. As soon as the limit conditions for one of the tests is met, data acquisition and all tests stop. To reset any of the limit tests, click Clear on the menu bar or change any of the following parameters: vertical scale, offset, horizontal position, horizontal scale, trigger settings, acquisition record length, or averaging.