<Name> Element

Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
L-SNT

Use this optional element to specify a measurement name that:

  • Appears on the measurement button that is placed on FlexDCA's User tab.
  • appears on the associated tab in the User Measurement Setup dialog.
  • Is returned by these SCPI remote queries:
    • :MEASure:EYE:USER:NAME?
    • :MEASure:OSCilloscope:USER:NAME?
    • :MEASure:TDR:USER:NAME?

Due to limited space on the measurement button, the name string is limited in length to 15 characters. Use the <Abbreviation> element to enter a shortened measurement name that appears on FlexDCA's measurement Results panel. Use the optional <Icon> element to place a custom picture on the button. If this element is missing from the XML file, the default name is the first 15 characters of the script file's name.

  • <Name>Pre-Emphasis</Name>

Parent Elements

<Measurement>

Child Elements

None

Attributes

None

Example

  • <Measurement>
  • …
  • <Name>My Eye MEas</Name>
  • <Abbreviation>MyEye</Abbreviation>
  • <Icon>EyeMeasBtn.png</Icon>
  • …
  • …
  • </Measurement>