<Script> Element

Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
L-SNT

Use this element to specify the Matlab or Python script to run. The filename extension (.m, .exe, or .py) must be included. A path is required if the script is located in a folder other than the default \User Measurements folder. The script can be based on any of the following file types that you create:

  • MATLAB scripts (*.m)
  • MATLAB Standalone Application (*.exe)
  • Python scripts (*.py)

Parent Elements

Child Elements

None

Attributes

None

Example

  • <Measurement>
  • …
  • <Script>EyeMeasurement.m</Script>
  • …
  • </Measurement>