<ValidMode> Element
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
L-SNT
Use this element to specify which FlexDCA mode the script is designed to work in. If FlexDCA is not in the specified mode when the user measurement is started, a messege is displayed. Only on mode can be specifie.
FlexDCA Mode | Element Example |
---|---|
Oscilloscope | <ValidMode>Scope</ValidMode> |
Eye/Mask | <ValidMode>Eye</ValidMode> |
TDR/TDT | <ValidMode>TDR</ValidMode> |
Jitter | Not supported by user measurements. |
Parent Elements
Child Elements
None
Attributes
None
Example
- <Measurement>
- …
- <ValidMode>Eye</ValidMode>
- <ValidMode>Eye,Scope</ValidMode> # invalid! Only one mode allowed.
- …
- …
- </Measurement>