<Comments> Element

Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
L-SNT

Use this optional element to specify an shortened measurement name to display on FlexDCA's measurement results table. The abbreviated measurement name also appears on the associated tab in the User Measurement Setup dialog. The abbreviated name string is limited in length to 15 characters. If this element is missing in the XML file, the default abbreviation is the name specified by the <Name> element.

  • <Abbreviation>EyeMeas</Abbreviation>

Parent Elements

Child Elements

None.

Attributes

None.

Example

  • <Measurement>
  • <Name>3rd Order Fltr</Name>
  • <Abbreviation>3rdFltr</Abbreviation>
  • …
  • …
  • </Measurement>