Test Program (Fixture Settings)
 
                                            In the Test Program Measurement Setup and Test Line Setup dialogs, the Fixture Lanes, Impairment, and User Measurement settings made.
Fixture Lanes
Select one or more Fixture Lanes to which dialog selections apply.
Impairments
If the test setup includes an Impairment block, as shown in this screen capture, you can select the impairment to be included (selected) or excluded (cleared) from the measurement path. Notice that the Impairment in the above dialog has been given the custom name "Fiber Spool". This was accomplished by clicking on the Impairment block in the Hardware Diagram.
User Measurements
If the test setup includes an Instrument block (for User Measurements), you can select the User Measurement to be included (selected) or excluded (cleared) in the lane measurements. When a User Measurement is selected for a Fixture's Lane, multiple Test Program lines are created. The first line is for the standard FlexOTO measurements. An additional test line is created for each selected User Measurement.