:CALibrate:RESPonse:CANCel
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:CANCel
Description
Cancels a JTF Response calibration that is in process. During a calibration, message or decision dialogs often appear and this command is equivalent to clicking the dialog's Cancel button. Use the :CALibrate:RESPonse:CONTinue command for an equivalent of the Next button. Use the :CALibrate:RESPonse:SDONe command to pause your application until the user clicks a button and to determine which button was pressed.
Requires FlexPLL revision A.06.70 and above.