:CALibrate:RESPonse:CDATa:STATus?
Flex Apps:
FlexPLL
Query Syntax
:CALibrate:RESPonse:CDATa:STATus?
Query Response
{CORR | INV}
Description
Returns the status of the Response calibration. INV is returned if calibration is not loaded or is not valid. CORR is returned if a Response calibration is loaded and ready to use. Use the :CALibrate:RESPonse:CDATa:STATus:REASon? query to determine why a calibration is invalid. If the calibration is invalid, perform a response calibration.
Requires FlexPLL revision A.06.70 and above.