:CALibrate:RESPonse:LOAD:STATe
Flex Apps:
FlexPLL
Query Syntax
:CALibrate:RESPonse:LOAD?
Query Response
{0 | 1}
Description
Queries the state of the JTF Response calibration in memory. A "0" is returned if calibration data is not in memory, and a "1" is returned if calibration data is in memory. Use the :CALibrate:RESPonse:LOAD command to load calibration data into memory from a file.
Requires FlexPLL revision A.06.70 and above.