:CALibrate:RESPonse:SNAMe
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:SNAMe
Description
Sets the file name prefix that is applied when FlexPLL automatically saves a Response calibration. The current date is appended to the prefix. The file name extension is always .jtfx. The default file name prefix is JTF_Cal. Any custom prefix is reset to the default string when a Default Setup is performed. This command supports the DEFault common child command.
The standard file name assigned to a file includes the date and an autonumber in the following form:
JTF_Cal_<date><autonumber>.jtfx
For example, JTF_Cal_2020-12-04_1.jtfx.
If an autonumber is used, the autonumber must be at the end of the file name, before the file name extension, and must begin with a hyphen followed by decimal digits.
| Name | Type | Autonumber |
|---|---|---|
| JTF_Cal_2017-04-08_1.jtfx | default | yes |
| DUT_A.jtfx | custom | no |
| DUT_A23.jtfx | custom | no |
| DUT_A_23.jtfx | custom | yes |