:CALibrate:RESPonse:CONTinue
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:CONTinue
Description
Continues a Response calibration that is in process. As a Response calibration progresses, message or decision dialogs often appear. For example, the user might be instructed to disconnect any front-panel inputs to a module. This command is equivalent to clicking the dialog's Next or Done button. Use the CALibrate:RESPonse:CANCel command for an equivalent of the Cancel button. Use the :CALibrate:RESPonse:SDONe command to pause your application until the user clicks a button and to determine the which button was pressed.
Requires FlexPLL revision A.06.70 and above.