:CALibrate:RESPonse:LOAD
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:LOAD
Description
Loads a previously saved JTF Response calibration file into memory. This is equivalent to clicking Load in the Response tab of the Calibration dialog. Before loading the file, you must specify the filename using the :CALibrate:RESPonse:LOAD:FNAMe command. To determine if a calibration has already been loaded into memory, use the :CALibrate:RESPonse:LOAD:STATe command.
Requires FlexPLL revision A.06.70 and above.