:CALibrate:RESPonse:CRECovery:LOAD:ENABled?
Flex Apps:
FlexPLL
Query Syntax
:CALibrate:RESPonse:CRECovery:LOAD:ENABled?
Description
Use this query to determine if there are any clock data recovery settings that need to be updated to match the loaded calibration. To update the settings, use the :CALibrate:RESPonse:CRECovery:LOAD command. This query is associated with the Load CDR Settings button in the Calibrations dialog.
| Returned Value |
CDR Settings | Associated Dialog Button |
|---|---|---|
| 1 | Need to be updated |
|
| 0 | Match |
|
Requires FlexPLL revision A.06.81 and above.