:CALibrate:RESPonse:ENABle
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:ENABle {ON | OFF}
Query Syntax
:CALibrate:RESPonse:ENABle?
Description
Enables or disables the currently loaded JTF Response calibration. This is equivalent to clicking Enable Response Calibration in the Response tab of the Calibration dialog. When disabled, the calibration remains in memory, so if instead you want to delete the calibration from memory, use the CALibrate:RESPonse:CLEarcommand.
Requires FlexPLL revision A.06.70 and above.