:CALibrate:RESPonse:JSOurce:LOAD
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:RESPonse:JSOurce:LOAD
Description
For an loaded JTF Response calibration (Response tab of Calibrations dialog), copies the calibration's Jitter Source settings into the Source Setup dialog. FlexPLL's current settings must match FlexPLL's settings at the time when the calibration file was created. Otherwise, the calibration will be invalid. This feature offers a quick method of configuring FlexPLL when importing a JTF response calibration file. To determine if the setting match the calibration file, use the :CALibrate:RESPonse:JSOurce:LOAD:ENABled query.
To match the clock-recovery Receiver settings, use the :CALibrate:RESPonse:CRECovery:LOAD command.
Requires FlexPLL revision A.06.70 and above.