:RMEMory:PLLModel:JTF:DISPlay
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1:4}:PLLModel:JTF:DISPlay {ON | OFF}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:DISPlay:MJTF.
Query Syntax
:RESPonse{1:4}:PLLModel:JTF:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the selected Response Memory's Model JTF plot on the JTF graph on or off. If the :RESPonse:DISPlay parent command is set to OFF, this command will not be able to display the JFT plot.
Example Command
:RMEMory2:PLLModel:JTF:DISPlay ON