:RMEMory:PLLModel:OJTf:DISPlay
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1:4}:PLLModel:OJTf:DISPlay {ON | OFF}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory:PLLModel:OJTf:DISPlay.
Query Syntax
:RMEMory{1:4}:PLLModel:OJTf:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the selected Response Memory's Model OJTF plot on the JTF graph on or off. If the :RMEMory:DISPlay parent command is set to OFF, this command will not be able to display the OJFT plot.
Example Command
:RMEMory2:PLLModel:OJTf:DISPlay ON