:RESPonse:PLLModel:OJTf:DISPlay
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:OJTf:DISPlay {ON | OFF}
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Query Syntax
:RESPonse{1}:PLLModel:OJTf:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the selected Response's Model OJTF plot on the JTF graph on or off. If the :RESPonse:DISPlay parent command is set to OFF, this command will not be able to display the OJFT plot.
Example Command
:RESPonse1:PLLModel:OJTf:DISPlay ON