:RMEMory:AVAilable?
Flex Apps:
FlexPLL
Query Syntax
:RMEMory{1:4}:AVAilable?
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3.
Description
Queries the state of a Response memory. :RMEMory:AVAilable? returns a 1 if a response is loaded in the indicated memory or return a 0 if the memory is empty. If the memory is available, you can display it's response on the JFT graph with the :RMEMory:DISPlay command or clear the memories contents with the :RMEMory:CLEar command.
Example Command
:RMEMory2:AVAilable?