:RESPonse:PLLModel:MEASure:DISPlay

Flex Apps:
FlexPLL

Command Syntax

:RESPonse{1}:PLLModel:MEASure:DISPlay {ON | OFF}

Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.

Query Syntax

:RESPonse{1}:PLLModel:MEASure:DISPlay?

Query Response

{1 | 0}

Description

Turns the display of the Response's model measurements in the results table on or off. If the :RESPonse:DISPlay parent command is set to OFF, this command will not be able to display the measurements.

Model Measurement's Effect on Measurements Displayed
Measurement :RESPonse:PLLModel:MEAS:DISPlay
Command
OFF ON
Maximum 1 ■ ■
Minimum 1 ■ ■
Average 1 ■ ■
Bandwidth ■ ■
Peaking ■ ■
Gain Frequency ■
Zero Frequency ■
Pole Frequency ■
Footnotes:
1. Displayed if :RESPonse:FLATness:MEASure:DISPlay command ON.

Example Command

:RESPonse1:PLLModel:MEASure:DISPlay ON