:RESPonse:PLLModel:MLOop:FPOLe
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:MLOop:FPOLe <loop pole>
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Where <loop pole> is a double.
Query Syntax
:RESPonse{1}:PLLModel:MLOop:FPOLe?
Description
Sets the frequency for the PLL loop pole for manually calculating the Response JTF and OJTF models. The loop pole is the single frequency in the JTF model where gain increases. The default value is 20 GHz, the minimum value is 1 Hz, and the maximum value is 1.00 THz.
Use the :RESPonse:PLLModel:ALOop:ENABle command to allow manual configuration of the JFT and OJTF models.
with Zero, Pole, and Gain Frequencies
Example Command
:RESPonse1:PLLModel:MLOop:FPOLe 2.0E+10