:RESPonse:UNAMe

Flex Apps:
FlexPLL

Command Syntax

:RESPonse{1}:UNAMe "<string>"

Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.

Query Syntax

:RESPonse{1}:UNAMe?

Description

Assigns a custom user name to the Response plots on the JTF graph. The default name is "Response 1". User names are displayed on the screen and on screen captures. To return a user name to its default value, send an empty string with this command.

The maximum length of the custom name is 255 characters.

Example Command

:RESPonse:UNAMe "DUT 18"