:RESPonse Subsystem
Flex Apps:
FlexPLL
The :RESPonse (Response) subsystem allows you to change the manner in which the Response plots (JTF, JTF modeled, and OJTF modeled) are displayed. This includes turning the display of the graphs on or off, changing their color, or giving the Response plots a custom name. To perform these tasks on Response Memory plots, use the commands in the :RMEMory subsystem.
In addition, the commands under the :RESPonse:PLLModel node select whether the PLL loop settings for calculating the Response models are automatically or manually selected (:RESPonse:PLLModel:ALOop:ENABle). When manually selected, use the following commands to configure the settings:
- Loop Gain (
:RESPonse:PLLModel:MLOop:FGAin) - Loop Zero (
:RESPonse:PLLModel:MLOop:FZERo) - Loop Pole (
:RESPonse:PLLModel:MLOop:FPOLe) - Loop Q Factor (
:RESPonse:PLLModel:MLOop:QFACtor)