:RESPonse:PLLModel:ALOop:ENABle
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:ALOop:ENABle {ON | OFF}
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Query Syntax
:RESPonse{1}:PLLModel:ALOop:ENABle?
Description
Enables ON or disables OFF the automatic calculation the model loop parameters given the DUT's PLL order entered using the :RESPonse:PLLModel:DUT:LORDer command. The loop order that you select is applied to automatically and manually calculated models. Turn this setting OFF if you want to manually enter the loop parameters settings with these commands:
- Loop fGain (
:RESPonse:PLLModel:MLOop:FGAin) - Loop fZero (
:RESPonse:PLLModel:MLOop:FZERo) - Loop fPole (
:RESPonse:PLLModel:MLOop:FPOLe)
When entering parameters to manually calculate the models, you can start by copying the current automatically calculated parameters in the manual settings using the :RESPonse:PLLModel:ALOop:COPY command.
Example Command
:RESPonse1:PLLModel:ALOop:ENABle ON