:RESPonse:PLLModel:MLOop:FGAin
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:MLOop:FGAin <loop gain>
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Where <loop gain> is a double.
Query Syntax
:RESPonse{1}:PLLModel:MLOop:FGAin?
Description
Sets the frequency for the PLL loop gain for manually calculating the Response JTF and OJTF model plots. Loop gain is the frequency at which the model JTF and OJTF curves intersect. The default value is 3.00 MHz, the minimum value is 1 Hz, and the maximum value is 1.00 THz.
Use the :RESPonse:PLLModel:ALOop:ENABle command to allow manual configuration of the JFT and OJTF models.
with Zero, Pole, and Gain Frequencies
Example Command
:RESPonse1:PLLModel:MLOop:FGAin 3.0E+6