:RESPonse:PLLModel:DUT:LORDer
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:DUT:LORDer {FIRSt | SECond | THIRd | FOURth}
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Query Syntax
:RESPonse{1}:PLLModel:DUT:LORDer?
Description
Specifies the DUT's PLL order as being First, Second, Third, or Fourth. The loop order that you select is applied to automatically and manually calculated Response models.
Example Command
:RESPonse1:PLLModel:DUT:LORDer SECond