:RESPonse:PLLModel:ENABle
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:PLLModel:ENABle {ON | OFF}
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Query Syntax
:RESPonse{1}:PLLModel:ENABle?
Description
Enables ON or disables OFF the creation of Model JTF and Model OJTF plots. By default the FlexPLL automatically calculates the DUT's loop parameters based on a Third order phase locked loop. Turning this setting OFF prevents the display of JTF and OJTF models.
When this setting is turned on, use the following commands to enable or disable the viewing of the Models and parameters:
- Model JTF (
:RESPonse:PLLModel:JTF:DISPlay) - Model OJTF (
:RESPonse:PLLModel:OJTF:DISPlay) - Model measurements (
:RESPonse:PLLModel:MEASure:DISPlay)
To configure the JTF and OJTF models, use the following commands:
- Enter the DUT's PLL order using the
:RESPonse:PLLModel:DUT:LORDercommand. - Select automatic (default) or manual calculation of the models with the
:RESPonse:PLLModel:ALOop:ENABlecommand.
Example Command
:RESPonse1:PLLModel:ENABle ON