:FUNCtion:EYE:CCOunt

Command Syntax

:FUNCtionN:EYE:CCOunt <num_hits>
            

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<num_hits> is an integer.

Query Syntax

:FUNCtionN:EYE:CCOunt?

Description

This command specifies the minimum highest hit count in the real-time eye's color grade - gray scale database that must occur before making measurements on the data. Increasing this value lets more waveforms be collected before making measurements, thereby increasing measurement accuracy. The default value for this control is 1.