:FUNCtion:EYE:XPOSition
Command Syntax
:FUNCtionN:EYE:XPOSition <time>
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
<time> is a double.
Query Syntax
:FUNCtionN:EYE:XPOSition?
Description
Sets the function N horizontal time position (center display location) of the real-time eye display.
This command directly affects the real-time eye's horizontal position setting in UI (unit interval) units (see the :FUNCtion:EYE:UIXPosition command).
To set the horizontal time scale of the real-time eye display in seconds-per-division, use the :FUNCtion:EYE:XSCale command.