:FUNCtion:EYE:CURSor

Command Syntax

:FUNCtionN:EYE:CURSor <symbol_0_position>
            

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<symbol_0_position> is an integer from 0 to 15.

Query Syntax

:FUNCtionN:EYE:CURSor?

Description

When qualifying a real-time eye with symbols in a 16-character pattern (see :FUNCtion:EYE:BITS), this command selects the position of symbol 0 in the pattern. Depending on which position you select for symbol 0, the pattern can include symbols before, after, or both before and after symbol 0. Position 0 means all symbols in the pattern are before symbol 0. Position 15 means all symbols in the pattern are after symbol 0.

To specify the pattern, see the :FUNCtion:EYE:PATTern command.