:FUNCtion:EYE:UIXPosition

Command Syntax

:FUNCtionN:EYE:UIXPosition <time_in_UI>
            

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<time_in_UI> is a double in UI (unit interval) units.

Query Syntax

:FUNCtionN:EYE:UIXPosition?

Description

Sets the function N horizontal time position (center display location) of the real-time eye display in UI units.

This command directly affects the real-time eye's horizontal position setting in seconds (see the :FUNCtion:EYE:XPOSition command).

To set the horizontal time range of the real-time eye display in UI units, use the :FUNCtion:EYE:UIXRange command.