:FUNCtion:EYE:XSCale

Command Syntax

:FUNCtionN:EYE:XSCale <seconds_per_div>
            

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<seconds_per_div> is a double.

Query Syntax

:FUNCtionN:EYE:XSCale?

Description

Sets the function N horizontal time scale of the real-time eye display in seconds-per-division.

This command directly affects the real-time eye's horizontal range setting in UI (unit interval) units (see the :FUNCtion:EYE:UIXRange command).

To set the horizontal position (center display location), use the :FUNCtion:EYE:XPOSition command.

Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.