:FUNCtion:EYE:UUNits

Command Syntax

:FUNCtionN:EYE:UUNits {UINTerval | SECond}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:EYE:UUNits?

Query Response

{UINT | SEC}

Description

This command specifies the user interface's units option for the real-time eye horizontal Scale and Position controls. You can select either Unit Intervals (UIs) or time (in seconds).

To specify the real-time eye horizontal scale and position in terms of UI units, use the :FUNCtion:EYE:UIXRange and :FUNCtion:EYE:UIXPosition commands.

To specify the real-time eye horizontal scale and position in terms of time units, use the :FUNCtion:EYE:XSCale and :FUNCtion:EYE:XPOSition commands.