:FUNCtion:EYE:DISPlay

Command Syntax

:FUNCtionN:EYE:DISPlay {ON | OFF | 1 | 0}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:EYE:DISPlay?

Query Response

{1 | 0}

Description

Turns the display of the specified function's real-time eye on or off. Use the :FUNCtion:STATus? command to determine if a function is available for display.

Use an *OPC (Operation Complete) query to pause program execution while waiting for this command to complete.