:FUNCtion:EYE:UIXRange
Command Syntax
:FUNCtionN:EYE:UIXRange <time_in_UI>
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
<time_in_UI> is a double in UI (unit interval) units.
Query Syntax
:FUNCtionN:EYE:UIXRange?
Description
Sets the function N horizontal time range (width) of the real-time eye display in UI units.
This command directly affects the real-time eye's horizontal time/div setting in seconds (see the :FUNCtion:EYE:XSCale command).
To set the horizontal position (center display location) of the real-time eye display in UI units, use the :FUNCtion:EYE:UIXPosition command.
Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.