:FUNCtion:EYE:CWINdow
Command Syntax
:FUNCtionN:EYE:CWINdow TIME{1:4}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:EYE:CWINdow?
Description
The :FUNCtion:EYE:CWINdow command lets you assign a real-time eye waveform to a Waveform content window.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIME{1:4} | Waveform | 4 | 4 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |