Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MARKers:MARKer{N}:CENTer

:MARKers Commands
  • :MARKers Subsystem
  • :MARKers:FPBPress
  • :MARKers:HIDE
  • :MARKers:MARKer{N}:CENTer
  • :MARKers:MARKer{N}:DELete
  • :MARKers:MARKer{N}:IDELta
  • :MARKers:MARKer{N}:IXDelta?
  • :MARKers:MARKer{N}:IXDelta:STATus?
  • :MARKers:MARKer{N}:IXDelta:STATus:REASon?
  • :MARKers:MARKer{N}:MNAMe
  • :MARKers:MARKer{N}:SCOPe
  • :MARKers:MARKer{N}:SOURce
  • :MARKers:MARKer{N}:STATe
  • :MARKers:MARKer{N}:TVALue?
  • :MARKers:MARKer{N}:TVALue:STATus?
  • :MARKers:MARKer{N}:TVALue:STATus:REASon?
  • :MARKers:MARKer{N}:TYPE
  • :MARKers:MARKer{N}:X
  • :MARKers:MARKer{N}:XDELta?
  • :MARKers:MARKer{N}:XDELta:STATus?
  • :MARKers:MARKer{N}:XDELta:STATus:REASon?
  • :MARKers:MARKer{N}:XDPos
  • :MARKers:MARKer{N}:XDText
  • :MARKers:MARKer{N}:Y
  • :MARKers:MARKer{N}:YDELta?
  • :MARKers:MARKer{N}:YDELta:STATus?
  • :MARKers:MARKer{N}:YDELta:STATus:REASon?
  • :MARKers:MARKer{N}:YDPos
  • :MARKers:MARKer{N}:YDText
  • :MARKers:MINTensity
  • :MARKers:MRESults
  • :MARKers:OFF
  • :MARKers:SHOW

Command Syntax

:MARKers:MARKer{N}:CENTer
Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.

Description

This command changes the grid's horizontal position in order to center the marker. This can change the horizontal position in other grids as well.

This command performs the same operation as the Position Display to Center Marker button in the graphical user interface's Markers dialog box.