:MARKers:MARKer{N}:Y
:MARKers Commands
- :MARKers Subsystem
- :MARKers:FPBPress
- :MARKers:HIDE
- :MARKers:MARKer{N}:CENTer
- :MARKers:MARKer{N}:DELete
- :MARKers:MARKer{N}:IDELta
- :MARKers:MARKer{N}:IXDelta?
- :MARKers:MARKer{N}:IXDelta:STATus?
- :MARKers:MARKer{N}:IXDelta:STATus:REASon?
- :MARKers:MARKer{N}:MNAMe
- :MARKers:MARKer{N}:SCOPe
- :MARKers:MARKer{N}:SOURce
- :MARKers:MARKer{N}:STATe
- :MARKers:MARKer{N}:TVALue?
- :MARKers:MARKer{N}:TVALue:STATus?
- :MARKers:MARKer{N}:TVALue:STATus:REASon?
- :MARKers:MARKer{N}:TYPE
- :MARKers:MARKer{N}:X
- :MARKers:MARKer{N}:XDELta?
- :MARKers:MARKer{N}:XDELta:STATus?
- :MARKers:MARKer{N}:XDELta:STATus:REASon?
- :MARKers:MARKer{N}:XDPos
- :MARKers:MARKer{N}:XDText
- :MARKers:MARKer{N}:Y
- :MARKers:MARKer{N}:YDELta?
- :MARKers:MARKer{N}:YDELta:STATus?
- :MARKers:MARKer{N}:YDELta:STATus:REASon?
- :MARKers:MARKer{N}:YDPos
- :MARKers:MARKer{N}:YDText
- :MARKers:MINTensity
- :MARKers:MRESults
- :MARKers:OFF
- :MARKers:SHOW
Command Syntax
:MARKers:MARKer{N}:Y{1|2} <Y_value>Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.<Y_value> is a double.
Query Syntax
:MARKers:MARKer{N}:Y{1|2}?Description
For Y marker types (see :MARKers:MARKer{N}:TYPE), this command specifies the marker's Y location in the source waveform grid. In the case of delta Y marker types, this command specifies two marker Y locations (Y1) and (Y2).