:MARKers:MARKer{N}:XDELta:STATus?
Query Syntax
:MARKers:MARKer{N}:XDELta{1:4}:STATus?Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.Query Response
{CORR | INV | QUES}- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the :MARKers:MARKer{N}:XDELta? measurement. Use the :MARKers:MARKer{N}:XDELta:STATus:REASon? query to determine the reason for an invalid or questionable measurement.