:MARKers:MARKer{N}:SCOPe
Command Syntax
:MARKers:MARKer{N}:SCOPe {SIGNal | CWINdow | GLOBal}Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.Query Syntax
:MARKers:MARKer{N}:SCOPe?Description
This command specifies where the marker is displayed:
SIGNal— The marker is displayed only in the grid containing the source waveform.CWINdow— The marker is displayed in all the grids of the source waveform's content window.GLOBal— The marker is global and is displayed across all waveform content windows with compatible axes.
The Delta Marker types (see :MARKers:MARKer{N}:TYPE) allow only the SIGNal option.