Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MARKers:MINTensity

:MARKers Commands
  • :MARKers Subsystem
  • :MARKers:FPBPress
  • :MARKers:HIDE
  • :MARKers:MARKer{N}:CENTer
  • :MARKers:MARKer{N}:DELete
  • :MARKers:MARKer{N}:IDELta
  • :MARKers:MARKer{N}:IXDelta?
  • :MARKers:MARKer{N}:IXDelta:STATus?
  • :MARKers:MARKer{N}:IXDelta:STATus:REASon?
  • :MARKers:MARKer{N}:MNAMe
  • :MARKers:MARKer{N}:SCOPe
  • :MARKers:MARKer{N}:SOURce
  • :MARKers:MARKer{N}:STATe
  • :MARKers:MARKer{N}:TVALue?
  • :MARKers:MARKer{N}:TVALue:STATus?
  • :MARKers:MARKer{N}:TVALue:STATus:REASon?
  • :MARKers:MARKer{N}:TYPE
  • :MARKers:MARKer{N}:X
  • :MARKers:MARKer{N}:XDELta?
  • :MARKers:MARKer{N}:XDELta:STATus?
  • :MARKers:MARKer{N}:XDELta:STATus:REASon?
  • :MARKers:MARKer{N}:XDPos
  • :MARKers:MARKer{N}:XDText
  • :MARKers:MARKer{N}:Y
  • :MARKers:MARKer{N}:YDELta?
  • :MARKers:MARKer{N}:YDELta:STATus?
  • :MARKers:MARKer{N}:YDELta:STATus:REASon?
  • :MARKers:MARKer{N}:YDPos
  • :MARKers:MARKer{N}:YDText
  • :MARKers:MINTensity
  • :MARKers:MRESults
  • :MARKers:OFF
  • :MARKers:SHOW

Command Syntax

:MARKers:MINTensity  <intensity>

<intensity> is an integer.

Query Syntax

:MARKers:MINTensity?

Description

This command adjusts the brightness of all marker information on the display.

You can adjust the marker intensity between the values of 0% (minimal brightness) to 100% (full brightness). The default value is 80%.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.