:MARKers:MARKer{N}:TVALue:STATus?

Query Syntax

:MARKers:MARKer{N}:TVALue{1|2}:STATus?
Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the :MARKers:MARKer{N}:TVALue? measurement. Use the :MARKers:MARKer{N}:TVALue:STATus:REASon? query to determine the reason for an invalid or questionable measurement.

See Also