:MARKers:MARKer{N}:XDELta:STATus:REASon?
:MARKers Commands
- :MARKers Subsystem
- :MARKers:FPBPress
- :MARKers:HIDE
- :MARKers:MARKer{N}:CENTer
- :MARKers:MARKer{N}:DELete
- :MARKers:MARKer{N}:IDELta
- :MARKers:MARKer{N}:IXDelta?
- :MARKers:MARKer{N}:IXDelta:STATus?
- :MARKers:MARKer{N}:IXDelta:STATus:REASon?
- :MARKers:MARKer{N}:MNAMe
- :MARKers:MARKer{N}:SCOPe
- :MARKers:MARKer{N}:SOURce
- :MARKers:MARKer{N}:STATe
- :MARKers:MARKer{N}:TVALue?
- :MARKers:MARKer{N}:TVALue:STATus?
- :MARKers:MARKer{N}:TVALue:STATus:REASon?
- :MARKers:MARKer{N}:TYPE
- :MARKers:MARKer{N}:X
- :MARKers:MARKer{N}:XDELta?
- :MARKers:MARKer{N}:XDELta:STATus?
- :MARKers:MARKer{N}:XDELta:STATus:REASon?
- :MARKers:MARKer{N}:XDPos
- :MARKers:MARKer{N}:XDText
- :MARKers:MARKer{N}:Y
- :MARKers:MARKer{N}:YDELta?
- :MARKers:MARKer{N}:YDELta:STATus?
- :MARKers:MARKer{N}:YDELta:STATus:REASon?
- :MARKers:MARKer{N}:YDPos
- :MARKers:MARKer{N}:YDText
- :MARKers:MINTensity
- :MARKers:MRESults
- :MARKers:OFF
- :MARKers:SHOW
Query Syntax
:MARKers:MARKer{N}:XDELta:STATus:REASon?Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for an invalid or questionable :MARKers:MARKer{N}:XDELta? measurement. If the measurement was successful, a null string is returned. Use the :MARKers:MARKer{N}:XDELta:STATus? query to get the status of the measurement.