:MARKers:MARKer{N}:YDPos
:MARKers Commands
- :MARKers Subsystem
- :MARKers:FPBPress
- :MARKers:HIDE
- :MARKers:MARKer{N}:CENTer
- :MARKers:MARKer{N}:DELete
- :MARKers:MARKer{N}:IDELta
- :MARKers:MARKer{N}:IXDelta?
- :MARKers:MARKer{N}:IXDelta:STATus?
- :MARKers:MARKer{N}:IXDelta:STATus:REASon?
- :MARKers:MARKer{N}:MNAMe
- :MARKers:MARKer{N}:SCOPe
- :MARKers:MARKer{N}:SOURce
- :MARKers:MARKer{N}:STATe
- :MARKers:MARKer{N}:TVALue?
- :MARKers:MARKer{N}:TVALue:STATus?
- :MARKers:MARKer{N}:TVALue:STATus:REASon?
- :MARKers:MARKer{N}:TYPE
- :MARKers:MARKer{N}:X
- :MARKers:MARKer{N}:XDELta?
- :MARKers:MARKer{N}:XDELta:STATus?
- :MARKers:MARKer{N}:XDELta:STATus:REASon?
- :MARKers:MARKer{N}:XDPos
- :MARKers:MARKer{N}:XDText
- :MARKers:MARKer{N}:Y
- :MARKers:MARKer{N}:YDELta?
- :MARKers:MARKer{N}:YDELta:STATus?
- :MARKers:MARKer{N}:YDELta:STATus:REASon?
- :MARKers:MARKer{N}:YDPos
- :MARKers:MARKer{N}:YDText
- :MARKers:MINTensity
- :MARKers:MRESults
- :MARKers:OFF
- :MARKers:SHOW
Command Syntax
:MARKers:MARKer{N}:YDPos <horizontal_placement>Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.<horizontal_placement> is a double from 0 to 100.
Query Syntax
:MARKers:MARKer{N}:YDPos?Description
For Delta Y marker types (see :MARKers:MARKer{N}:TYPE), this command specifies the horizontal placement of the displayed value in the source waveform grid.
Use the :MARKers:MARKer{N}:YDText command to specify an optional description for the displayed value.