:MARKers:MARKer{N}:MNAMe
Command Syntax
:MARKers:MARKer{N}:MNAMe{1|2} <quoted_string>Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.<quoted_name> is a string.
Query Syntax
:MARKers:MARKer{N}:MNAMe{1|2}?Description
This command specifies the marker's name. The default name for a marker (MNAMe) or (MNAMe1) is its number.
In the case of delta marker types, this command specifies two names for the marker pair (MNAMe1) and (MNAMe2). The default name for the second marker (MNAMe2) is its number and the "prime" math symbol.