Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MARKers:MARKer{N}:X

:MARKers Commands
  • :MARKers Subsystem
  • :MARKers:FPBPress
  • :MARKers:HIDE
  • :MARKers:MARKer{N}:CENTer
  • :MARKers:MARKer{N}:DELete
  • :MARKers:MARKer{N}:IDELta
  • :MARKers:MARKer{N}:IXDelta?
  • :MARKers:MARKer{N}:IXDelta:STATus?
  • :MARKers:MARKer{N}:IXDelta:STATus:REASon?
  • :MARKers:MARKer{N}:MNAMe
  • :MARKers:MARKer{N}:SCOPe
  • :MARKers:MARKer{N}:SOURce
  • :MARKers:MARKer{N}:STATe
  • :MARKers:MARKer{N}:TVALue?
  • :MARKers:MARKer{N}:TVALue:STATus?
  • :MARKers:MARKer{N}:TVALue:STATus:REASon?
  • :MARKers:MARKer{N}:TYPE
  • :MARKers:MARKer{N}:X
  • :MARKers:MARKer{N}:XDELta?
  • :MARKers:MARKer{N}:XDELta:STATus?
  • :MARKers:MARKer{N}:XDELta:STATus:REASon?
  • :MARKers:MARKer{N}:XDPos
  • :MARKers:MARKer{N}:XDText
  • :MARKers:MARKer{N}:Y
  • :MARKers:MARKer{N}:YDELta?
  • :MARKers:MARKer{N}:YDELta:STATus?
  • :MARKers:MARKer{N}:YDELta:STATus:REASon?
  • :MARKers:MARKer{N}:YDPos
  • :MARKers:MARKer{N}:YDText
  • :MARKers:MINTensity
  • :MARKers:MRESults
  • :MARKers:OFF
  • :MARKers:SHOW

Command Syntax

:MARKers:MARKer{N}:X{1|2} <X_value>
Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.

<X_value> is a double.

Query Syntax

:MARKers:MARKer{N}:X{1|2}?

Description

For X marker types (see :MARKers:MARKer{N}:TYPE), this command specifies the marker's X location in the source waveform grid. In the case of delta X marker types, this command specifies two marker X locations (X1) and (X2).