Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MARKers:MARKer{N}:YDELta:STATus:REASon?

:MARKers Commands
  • :MARKers Subsystem
  • :MARKers:FPBPress
  • :MARKers:HIDE
  • :MARKers:MARKer{N}:CENTer
  • :MARKers:MARKer{N}:DELete
  • :MARKers:MARKer{N}:IDELta
  • :MARKers:MARKer{N}:IXDelta?
  • :MARKers:MARKer{N}:IXDelta:STATus?
  • :MARKers:MARKer{N}:IXDelta:STATus:REASon?
  • :MARKers:MARKer{N}:MNAMe
  • :MARKers:MARKer{N}:SCOPe
  • :MARKers:MARKer{N}:SOURce
  • :MARKers:MARKer{N}:STATe
  • :MARKers:MARKer{N}:TVALue?
  • :MARKers:MARKer{N}:TVALue:STATus?
  • :MARKers:MARKer{N}:TVALue:STATus:REASon?
  • :MARKers:MARKer{N}:TYPE
  • :MARKers:MARKer{N}:X
  • :MARKers:MARKer{N}:XDELta?
  • :MARKers:MARKer{N}:XDELta:STATus?
  • :MARKers:MARKer{N}:XDELta:STATus:REASon?
  • :MARKers:MARKer{N}:XDPos
  • :MARKers:MARKer{N}:XDText
  • :MARKers:MARKer{N}:Y
  • :MARKers:MARKer{N}:YDELta?
  • :MARKers:MARKer{N}:YDELta:STATus?
  • :MARKers:MARKer{N}:YDELta:STATus:REASon?
  • :MARKers:MARKer{N}:YDPos
  • :MARKers:MARKer{N}:YDText
  • :MARKers:MINTensity
  • :MARKers:MRESults
  • :MARKers:OFF
  • :MARKers:SHOW

Query Syntax

:MARKers:MARKer{N}:YDELta{1:4}{A:C}:STATus:REASon?
Where N identifies one of 16 possible markers {1:16}. For example, MARKer4.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for an invalid or questionable :MARKers:MARKer{N}:YDELta? measurement. If the measurement was successful, a null string is returned. Use the :MARKers:MARKer{N}:YDELta:STATus? query to get the status of the measurement.

See Also

  • Measurement Errors